Technical FAQs

Ask a Question

What is the trip level of the current unbalance protection on the 9065SS overload?<br />

The overload is supposed to not trip at 17% current imbalance and must trip in 3 seconds at 25%




CTA-ID : 2036993
Was this helpful?
What can we do to improve the information ?