Technical FAQs

Ask a Question

What is the catalog number for a connector cable for use with an XS630B1MAU20?<br />

XSZCK101Y is the 2 meter 90 degree connector cable and XSZCK111Y is the 2 meter straight cable that can be used with the XS630B1MAU20 sensor. These cables are also for use on the older XS..MA230 and XS..MA250 multi-voltage sensors. The ``K`` suffix on older sensors is identical, only the coding has been changed.


CTA-ID : 2036019
Was this helpful?
What can we do to improve the information ?