Technical FAQs

Ask a Question

Can you change a HJM36150 breaker to 100% rated?

No, cannot change standard 80% rated Powerpact breaker to 100% rated (``C``) in the field.


CTA-ID : 2037106
Was this helpful?
What can we do to improve the information ?