Technical FAQs

Ask a Question

What is the ambient temperature range for the 9007T and 9007FT type limit switches?

-10 degrees F ( -23 degrees C) and + 185 degrees F ( + 85 degrees C) Housing may withstand hot falling sand at 300 degrees F.


CTA-ID : 2037100
Was this helpful?
What can we do to improve the information ?