Technical FAQs

Ask a Question

Are the 2510KR and 2510FR factory sealed devices?

These are explosion proof, cast aluminum enclosed manual switches rated NEMA Types 3R, 7 and 9. They are intended for use in Division 1 & 2, Class 1 Groups B, C, D or Class 2 Groups E, F, G applications. These are not factory-sealed devices and therefore can be disassembled in order to replace the open style switch or other internal components. Conduit seal to be supplied by customer.


CTA-ID : 2037073
Was this helpful?
What can we do to improve the information ?