Technical FAQs

Ask a Question

Are UL489 listed Multi-9 breakers available in a 4 pole version?

No. UL489 listed Multi-9 breakers are available in 1, 2, and 3 pole versions only. For a 4 pole Multi-9 breaker, recommend the UL1077 version.


CTA-ID : 2037026
Was this helpful?
What can we do to improve the information ?