Technical FAQs

Ask a Question

What is the part number for a replacement fuse base assembly for a 9422TE2?

Replacement fuse base assembly is obsolete. There are two options:

1) Customer can use the fuse base part 40520-216-52 and re-use the mounting base.

2) Customer will need to replace switch and operating mechanism with a 9422TEF10.


CTA-ID : 2037008
Was this helpful?
What can we do to improve the information ?