Technical FAQs

Ask a Question

What is the fire containment rating for ALL Combination Service Entrance Devices?

Issue:
Product Ratings or features

Product Line:
Combination Service Entrance Devices

Environment:
Mounting location

Cause:
Application

Resolution:
Combination Service Entrance Devices(CSED) DO NOT have a Fire Containment Rating(or a fire wall rating). Applicable UL and NEMA standards do not address fire containments ratings for these products.




CTA-ID : 2036832
Was this helpful?
What can we do to improve the information ?