Technical FAQs

Ask a Question

Is a pulsation plug, Form P, available for all 9013 FHG pressure switches?

No, the pulsation plug, Form P, is only available for devices with the single 1/4`` NPSF (internal) thread pressure connection. It is not available on devices with the four way fitting, and it is available factory installed only. This device is not intended for use with pneumatic systems. This information may not be shown or reflected in our Digest.

CTA-ID : 2036957
Was this helpful?
What can we do to improve the information ?