Technical FAQs

Ask a Question

What is the amperage range of branch breakers that can be used in a RC816D200CH?

A 100A maximum branch breaker can be installed in the lowest position in the branch panel. All other positions are limited to 70A maximum branch circuit breaker.

CTA-ID : 2036938
Was this helpful?
What can we do to improve the information ?