Technical FAQs

Ask a Question

Is special hardware needed to adapt a 9422ATDF631 operating mechanism to use J type fuses?

No. To use ``J`` type fuses, the customer must move the trailer fuse base to the proper position. No additional hardware or rejection clips are needed.

CTA-ID : 2037012
Was this helpful?
What can we do to improve the information ?