Technical FAQs

Ask a Question

Are the QOB-HID type branch breakers rated for 22K AIC?

Issue:
Product design feature

Product Line:
QOB Branch breakers

Environment:
AIC rating

Cause:
Application

Resolution:
No. The QOB-HID type branch breakers are rated at 10K AIC maximum.


CTA-ID : 2036941
Was this helpful?
What can we do to improve the information ?