Technical FAQs

Ask a Question

What is the amperage range of branch breakers that can be used in a SC1624M125S?

A 125A maximum branch breaker can be installed in the top position in the branch panel. All other positions are limited to 100A maximum branch circuit breaker (#1 AWG maximum wire).


CTA-ID : 2036951
Was this helpful?
What can we do to improve the information ?