Technical FAQs

Ask a Question

XUZA218 swivel mounting bracket: Can the mount be used as adjustment?

Yes, the swivel allows 15 degrees of movement to allow alignment with target. Once adjustment is made, the bracket can be locked in place.

CTA-ID : 2036723
Was this helpful?
What can we do to improve the information ?