Technical FAQs

Ask a Question

Are there alarm auxiliary contacts available for the Bi metallic overload blocks, specifically a 9065SDO6B?<br />

No. The standard device does provide one Normally Open and one Normally Closed contact with a common point. No additional contacts can be added.


CTA-ID : 2035778
Was this helpful?
What can we do to improve the information ?