Technical FAQs

Ask a Question

What is the operational temperature range of the Integral starter?<br />

-20 to +60 degrees C for AC control and -25 to +50 degrees C for the DC control.


CTA-ID : 2035773
Was this helpful?
What can we do to improve the information ?