Technical FAQs

Ask a Question

What are the catalog numbers for the field-installable undervoltage shunt trip accessories for Powerpact DG, DJ, and DL type circuit breakers?

The field-installable shunt trip devices are as follows:
Volts AC        Suffix        Cat. #
24           SK           S29384  
48           SL           S29385  
110/130           SA           S29386  
208/277           SD           S29387  
380/480           SH           S29388  
525/600           SJ           S29389  

Volts DC        Suffix        Cat. #
12           SN           S29382  
24           SO           S29390  
30           SU           S29391  
48           SP           S29392  
60           SV           S29383  
125           SR           S29393  
250           SS           S29394  

CTA-ID : 2035681
Was this helpful?
What can we do to improve the information ?