Technical FAQs

Ask a Question

Verify part 48119-765-50 described as a solenoid, 48Vdc, type C, for motor operated Visi/Vac Circuit Interrupter

Per Neal Smith @ Smyrna, this is a good part number, not on Q2C. Order on Smyrna. This part number is an assembly that contains the 48VDC close or trip solenoid. The 48VDC solenoid alone is part number 44068-105-06.


CTA-ID : 2035696
Was this helpful?
What can we do to improve the information ?