Technical FAQs

Ask a Question

Will the horizontal and vertical hanger assemblies used on I-Line Busway accomodate All-thread as a hanging method?

Issue:
Will the horizontal and vertical hanger assemblies used on I-Line Busway accomodate All-thread as a hanging method?

Product Line:
I Line busway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes. All busway hangars are compatible with the use of All-thread.


CTA-ID : 2035637
Was this helpful?
What can we do to improve the information ?