Technical FAQs

Ask a Question

Can the CSED Value Pack SO2040VP be modified to flush or semi-flush mounting?

Issue:
Application

Product Line:
CSED

Cause:
Clarification of product application and features

Resolution:
No, the SO2040M200S provided in that Value Pack is designed for a surface mount application only.


CTA-ID : 2035621
Was this helpful?
What can we do to improve the information ?