Technical FAQs

Ask a Question

What are the replacement lugs for an EZM3600TB?<br /><br /><br />

The lug used on this device is part number 40251-136-50. There are two lugs used per phase and neutral.


CTA-ID : 2035584
Was this helpful?
What can we do to improve the information ?