Technical FAQs

Ask a Question

What is the maximum operating temperature on a PBQ3640G plug in unit?<br />

It is the same as the busway which is designed to operate at no more than 55 degree C above a 40 degree ambient.

CTA-ID : 2035503
Was this helpful?
What can we do to improve the information ?