Technical FAQs

Ask a Question

On a RC816F150CH, Series M01, what is the specified torque requirements for the incoming (line side) phase and neutral lugs?<br />

The line phase and neutral lugs wire binding screw should be torqued to 250 LB-IN.

CTA-ID : 2035063
Was this helpful?
What can we do to improve the information ?