Technical FAQs

Ask a Question

What is the difference between an old 9070 Type K and a new 9070 Type T?

The 9070T is CE rated, NOM approved, etc. and the Type K is obsolete and not available. The Type T replaces the Type K and matches in Function and Form, but not necessarily Fit (the dimensions may vary.)

CTA-ID : 2034976
Was this helpful?
What can we do to improve the information ?