Technical FAQs

Ask a Question

Does the SC40M200S accept tandem branch breakers?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Branch breakers

Cause:
Accepting Tandem breakers

Resolution:
NO, The SC40M200S contains a 40 full space load center that will only accept Full Size single pole or two pole breakers and will NOT accept tandem breakers.



CTA-ID : 2034963
Was this helpful?
What can we do to improve the information ?