Technical FAQs

Ask a Question

What is the wire range for the ZBE101 contact block terminal?

The terminals will accept :
Min: 1 X 24 AWG without cable end and 1 X 22 AWG for linking
Max: 2 X 16 AWG with cable end & 2 X 14 AWG w/o cable end.

CTA-ID : 2035456
Was this helpful?
What can we do to improve the information ?