Technical FAQs

Ask a Question

Are the joint bolts replaceable on I-Line II Busway?

Issue:
Are the joint bolts replaceable on I-Line II Busway?

Product Line:
I Line Busway

Environment:
Maintenance

Cause:
Repair/Replacement

Resolution:
Joint bolts are not available separately, however, a joint pack, which includes the joint bolts,  is available.


CTA-ID : 2035454
Was this helpful?
What can we do to improve the information ?