Technical FAQs

Ask a Question

What are the repair parts for the CH363RB series F5? (may be shown as F05)

The replacement parts for the CH363RB, series F5 (F05) are as follows. No other parts are available.

Interior kit - HSIF310F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Load base kit - HLB310F (includes load base & mounting hardware).
Arc Suppressor kit - HAS0610F - (includes arc suppressor & mounting hardware)
Lug kit - AL10F - (kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)



CTA-ID : 2035017
Was this helpful?
What can we do to improve the information ?