Technical FAQs

Ask a Question

Can an additional contact block be added to the XALK194 emergency stop control station?

Yes. There are provisions for 3 contact blocks. Use the base mount contacts, ZENL1111 normally open or ZENL1121 normally closed.

CTA-ID : 2035524
Was this helpful?
What can we do to improve the information ?