Technical FAQs

Ask a Question

What are the repair parts for the CH362RB series F5? (may be shown as F05)

Issue:
Current Design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The replacement parts for the CH362RB, series F5 (F05) are as follows. No other parts are available.

Interior kit - HSIF3606F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Load Base kit - HLB3606F (Includes load base & mounting hardware)
Arc Suppressor kit - HAS0610F(Includes arc suppressor & mounting hardware)
Lug kit - AL0306F (kit includes 6 lugs)
Handle/Mechanism kit- HM0610F(kit includes handle, mechanism, lockplate & mounting hardware)

 
Was this helpful?
What can we do to improve the information ?