Technical FAQs

Ask a Question

Can 240Vac fuse clips be used in the 600Vac QMB or QMJ switches?

Issue:
Product Design Features

Product Line:
QMB branch switches

Environment:
Fuse clips

Cause:
Application

Resolution:
No. 240Vac fuse clips can ONLY be used in 240Vac rated QMB/QMJ switches. The 600Vac max QMB/QMJ switches require the use of 600Vac fuses, but the 600Vac switch with the 600V fuses can be used at 240Vac. 


CTA-ID : 2035533
Was this helpful?
What can we do to improve the information ?