Technical FAQs

Ask a Question

Do HVL switches have any fault interrupting ratings?

No. The 600A switch will interrupt 600A thirty times. The 1200A switch will interrupt 1200A ten times. These ratings are per ANSI C37.22
The switch will do one closing on a fault and hold.


CTA-ID : 2035009
Was this helpful?
What can we do to improve the information ?