Technical FAQs

Ask a Question

What is the purpose of a MMLRK Anti-Inversion Kit?

This kit, when installed in th top right side meter jaw of a 400A CSED lever bypass meter socket, shall prevent Class 320 Watt-Hour meters from being installed upside down (inverted) and also rejects the use of Class 100 and Class 200 Watt-Hour meters.

CTA-ID : 2035145
Was this helpful?
What can we do to improve the information ?