Technical FAQs

Ask a Question

Is there a lug for 800A MGA breaker that will accept parallel 750 aluminum conductors?

There is no mechanical lug for Powerpact I-Line M-frame that will accept two 750 kcmil conductors, and compression lugs are not allowd on I-Line Powerpact breakers.


CTA-ID : 2035044
Was this helpful?
What can we do to improve the information ?