Technical FAQs

Ask a Question

Do 9070 industrial control transformers contain any materials, such as PCBs, lead, or other heavy metals, that would require special disposal means?

Square D 9070 Type T and TF industrial control transformers to not contain any material that would require any special disposal means and can be disposed of in the normal manner. However, the majority of the transformer`s material are recycleable (steel, copper,) and Square D urges the customer to recycle the unit if possible.

CTA-ID : 2035551
Was this helpful?
What can we do to improve the information ?