Technical FAQs

Ask a Question

Which are are the phase terminals and which is the neutral terminal on the HOM250GFI?

The middle silver terminal is the neutral and the two outside yellow screws are the phase terminals.

CTA-ID : 2035487
Was this helpful?
What can we do to improve the information ?