Technical FAQs

Ask a Question

On a SO2040M200S, Series M01, what is the specified torque requirements for the incoming (line side) phase and neutral lugs?

The line phase and neutral lugs wire binding screw should be torqued to 250 LB-IN.


CTA-ID : 2035142
Was this helpful?
What can we do to improve the information ?