Technical FAQs

Ask a Question

Why is Meter Main catalog number C125RB only rated at 10K if the QOM1-VH style breaker used with it is rated at 22K?

The enclosure used for this device is rated at 10K, even if the breaker used is 22K, because of UL testing restrictions. Use the CM200S and put a 100A QOM2 breaker in it, for a 22K rated device.

CTA-ID : 2035040
Was this helpful?
What can we do to improve the information ?