Technical FAQs

Ask a Question

Do 9007 type lever arms 9007HA3 or 9007HA7 have a steel roller?

The non-bendable HA3 and bendable HA7 do have steel rollers, but the non-bendable HA22 and bendable HA23 have nylon rollers which are lighter and more flexible. The nylon roller units are highly recommended for most applications, because of the long length of these lever arms, and the relatively greater weight of the steel roller type units.

CTA-ID : 2035525
Was this helpful?
What can we do to improve the information ?