Technical FAQs

Ask a Question

Will the QO220GFI operate with a split or duplex receptacle circuit? The split duplex receptacle has one line lead connected to the top outlet and the other line lead connected to the bottom outlet. Both hot leads at 120V return to the same neutral on that receptacle.

As long as all line and neutral conductors from that receptacle return to the hot and neutral connections at the off end of the GFI breaker, the GFI will operate correctly.

CTA-ID : 2035196
Was this helpful?
What can we do to improve the information ?