Technical FAQs

Ask a Question

Is the ZBW008 boot used on both the double headed operators with flush and extended operators?

Issue:
Is the ZBW008 boot used on both the double headed operators with flush and extended operators?

Product Line:
22mm Push Buttons

Environment:
XB4/XB5 22mm Push Buttons

Cause:
Clarify if different boots need to be ordered.                       

Resolution:                                                                 
Yes. The same boot is used for both device types.
 
Was this helpful?
What can we do to improve the information ?