Technical FAQs

Ask a Question

The F frame breakers are available in 240V, 480V, and 600V versions. Are the L frame breakers such as an LCL36600 available in a less expensive 240V or 480V version as well?

Breakers larger than 100A frame style are all available in the 600V version only. Consequently, there are no LA, LH, or LC frame breakers available in anything but 600V type.


CTA-ID : 2035151
Was this helpful?
What can we do to improve the information ?