Technical FAQs

Ask a Question

What is the quantity and wire size of the lugs in the PTB316GH and PTB316GV tap boxes?<br />

There are 6 lugs per phase and neutral with a wire size range of 2/0 to 600kcmil. There are also 2 lugs for the ground with a wire size range of 2/0 to 600kcmil



CTA-ID : 2035595
Was this helpful?
What can we do to improve the information ?