Technical FAQs

Ask a Question

What is the catalog number for the solid neutral that can be used with a MA1000R enclosure?

AL800SN is the solid neutral that can be used with a MA1000R enclosure.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2034915
Was this helpful?
What can we do to improve the information ?