Technical FAQs

Ask a Question

What are the part numbers for the red and black knob for the 9422A1 handle?

The black portion of the knob is 31008-038-01; the red portion of the knob is 31008-038-02; the rivet is 24102-12680

CTA-ID : 2035113
Was this helpful?
What can we do to improve the information ?