Technical FAQs

Ask a Question

Is the cover of a QO1612M125FTRB, QO816M150FTRB or QO1816M200FTRB load center side hinged or top hinged?

Issue:
Product design feature

Product Line:
QO Load Center

Cause:
Clarification of design feature

Resolution:
It is dependent upon the Series Number of the load center. 
The obsolete design, Series S01, is top hinged.
The current design, Series S02, is side hinged.


CTA-ID : 2035099
Was this helpful?
What can we do to improve the information ?