Technical FAQs

Ask a Question

Does Square D offer a Safety Socket Box with a test-bypass?

We currently offer two devices with a test block bypass:
Use EMT1200CB for a 120/240 Vac, 1-phase/3 wire, 225 ampere maximum application.
Use EMT3200CB for a 208Y/120 Vac or 240/120 Vac, 3-phase/4 wire, 225 ampere maximum application.
Refer to the latest Digest or Digest Plus Selector (on line) for further information.


CTA-ID : 2035153
Was this helpful?
What can we do to improve the information ?