Technical FAQs

Ask a Question

How far into the wall does a SU3040M225R install?

This device is a Reverse All-In-One, providing accessibility to the utility main lugs section, the meter socket and the main breaker on the exterior of the building and a 30 space/40 circuit load center on the interior of the building. It is 7.9`` deep. Of the 7.9``, 3.5`` will extend past the semi-flush flange (outside surface of the stud wall), 3.5`` will be in the wall cavity and .9`` will extend past the interior surface of the stud wall. Please refer to Approval Drawing #1965 for dimensional details.

CTA-ID : 2036067
Was this helpful?
What can we do to improve the information ?