Technical FAQs

Ask a Question

What Tenant Circuit Breakers can be used with a EZML113200 branch unit?

This device is now obsolete and replaced by catalog number: EZML113225 (rated 225A max. per tenant breaker position).
The previous 200A branch unit did make use of QE-VH style tenant circuit breakers (70A-200A max.), but they too are obsolete.
Contact 888-778-2733 for further assistance.


CTA-ID : 2036048
Was this helpful?
What can we do to improve the information ?