Technical FAQs

Ask a Question

Does the SC816F200S accept tandem or quad branch breakers?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Branch breakers

Cause:
Accepting Tandem breakers

Resolution:
Yes, The SC816F200S contains a 8space - 16 circuit load center and will accept up to 8 HOMT tandems or 4 HOMT quad branch breakers.


CTA-ID : 2036090
Was this helpful?
What can we do to improve the information ?